cancel
Showing results for 
Search instead for 
Did you mean: 

I would like to know the meaning of ADVdata in the (aci_gap_update_adv_data) function

fanyun
Associate II

Hello all.

I am currently testing the STEVAL-IDB008V1M development version, I am using the BlueNRG-2 example code (BLE_SensorDemo_BlueMSapp) and there is manuf_data[26] in the function (Set_DeviceConnectable) in the sensor.c file. Can anyone explain what the contents of this array stand for, I have checked the PM0257 and UM2071 files but they do not explain

Here is the content of the (Set_DeviceConnectable) function

void Set_DeviceConnectable(void)

{  

 uint8_t ret;

 uint8_t local_name[] = {AD_TYPE_COMPLETE_LOCAL_NAME,'B','l','u','e','N','R','G'}; 

  

 uint8_t manuf_data[26] = {

  2,0x0A,0x00 /* 0 dBm */, // Trasmission Power

  8,0x09,'B','l','u','e','N','R','G', // Complete Name

  13,0xFF,0x01, /*SKD version */

  0x04, /* 0x04: BlueNRG1-1/2 eval kits */

  0x00,

  0xD4, /* ACC+Gyro 0xC0 | 0x04 Temp | 0x10 Pressure*/

  0x00, /* */

  0x00, /* */

  0x00, /* BLE MAC start */

  0x00,

  0x00,

  0x00,

  0x00,

  0x00, /* BLE MAC stop */

 };

  

#if ST_OTA_FIRMWARE_UPGRADE_SUPPORT

 hci_le_set_scan_response_data(18,BTLServiceUUID4Scan); 

#else

 hci_le_set_scan_response_data(0,NULL);

#endif /* ST_OTA_FIRMWARE_UPGRADE_SUPPORT */ 

  

 PRINTF("Set General Discoverable Mode.\n");

  

 ret = aci_gap_set_discoverable(ADV_IND,

                (ADV_INTERVAL_MIN_MS*1000)/625,(ADV_INTERVAL_MAX_MS*1000)/625,

                 STATIC_RANDOM_ADDR, NO_WHITE_LIST_USE,

                 sizeof(local_name), local_name, 0, NULL, 0, 0); 

  

 aci_gap_update_adv_data(26, manuf_data);

  

 if(ret != BLE_STATUS_SUCCESS)

 {

  PRINTF("aci_gap_set_discoverable() failed: 0x%02x\r\n",ret);

  SdkEvalLedOn(LED3);  

 }

 else

  PRINTF("aci_gap_set_discoverable() --> SUCCESS\r\n");

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.