2022-03-24 9:04 PM
I designed a PCB with an STM32L476rc and a BlueNRG-2N, the buenrg is conected with usart3 and i want to read the bluenrg version and send it to usart2 to show it with docklight
please can someone give me a hand in the source code ,
2022-03-25 1:54 AM
HI @ZEya.1 ,
To discuss with BlueNRG-2N , you need to use predefined HCI/ACI commands.
ACI documentation for BlueNRG-2N is available in html format in STSW-BNRG2N-V320 package.
To get BeluNRG-2N version, you may use HCI_READ_LOCAL_VERSION_INFORMATION and ACI_HAL_GET_FIRMWARE_DETAILS.
Now, if you just started your project with BlueNRG-2N, I would strongly advise to use SPI link between BleuNRG-2N and STM32L476rc instead of UART.
Using SPI, a code example (similar to what you are doing) is already available : X-CUBE-BLE2
Regards,
Sebastien.
2022-03-25 4:39 AM
where i have to write the commands ! in the virtual terminal i put them ,, them then i get the version ? sorry i did not understand how i have to order my code
2022-03-25 5:10 AM
Hi @ZEya.1 ,
BlueNRG-2N is a network processor - already preflashed (including BLE certified BLE stack).
Supported commands (ACI/HCI) are described in html doc I pointed.
How to send command ? Here, outside BlueNRG-2N datasheet, there is also UM2805 : ACI command data format. Those documents explained what is BlueNRG-2N and how to send ACI/HCI commands to BlueNRG-2N over UART (or over SPI)
Now, as said in previous answer, if you have possibility to use SPI between your STM32L476 and BleuNRG-2N . I would strongly advise to start from X-CUBE-BLE2 package (only SPI supported). Code examples are for STM32L476 which is your target.
In terms of HW, it can be executed on NUCLOE-L476 + X-NUCLEO-BNRG2A1 expansion board (yhis expansion board emulate BleuNRG-2N )
Regards,
Sebastien.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.