2019-06-09 11:26 PM
Hello.
I want to use the Arduino Connectors on the STEVAL-STLCX01V1 board.
I know that i need to use the GPIO functions (in the "stm32l4xx_hal_gpio.c" library):
void HAL_GPIO_Init(GPIO_TypeDef *GPIOx, GPIO_InitTypeDef *GPIO_Init)
void HAL_GPIO_DeInit(GPIO_TypeDef *GPIOx, uint32_t GPIO_Pin)
void GPIO_PinState HAL_GPIO_ReadPin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin)
void HAL_GPIO_WritePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin, GPIO_PinState PinState)
void HAL_GPIO_TogglePin(GPIO_TypeDef* GPIOx, uint16_t GPIO_Pin)But i don't know how to use them. I mean, for example, if i want to use the D2 pin in the CN9 Arduino Connectors, what do i write in the GPIOx and GPIO_Pin variable?
How do i know which pin in the Arduino Connectors correspond to it's GPIOx and GPIO_Pin variable?
Also, after i know the GPIOx and GPIO_Pin that i want to use, how do i use them? i mean, which functions do i use to operate those pins?
Thank you for your help,
Reshef Finkelstein
2019-06-09 11:41 PM
The pins are usually described in the manual or expressed via a schematic. The arduino software hides this stuff in a board specific pin table.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.