2018-06-25 11:54 PM
I'm using BlueNRG-2 in Network Coprocessor mode over the SPI interface. After establishing a connection with my device, how can I tell if the remote device supports Data Length Extension?
I've experimented with the ACI_GATT_EXCHANGE_CONFIG command but that negotiates the max ATT_MTU size for L2CAP but the Response Event doesn't tell you anything about the Link Layer data size and if Data Length Extension is being used. Is there a way to find out?
2018-06-27 6:45 PM
Hi Shaq,
Could you check how the device responses to LL_FEATURES_REQ and LL_LENGTH_REQ?
Thank you.
Best Regards,
Winfred
2018-07-31 10:47 PM
I figured it out. Shortly after I posted my question, I noticed the new v2.1 FW was posted along with new documentation. The new release had new commands for negotiating larger ATT_MTU and Link Layer PDUs.
First step for a client is to send an ACI_GATT_EXCHANGE_CONFIG command so that both ends negotiate their max MTU. I noticed Android phones will not turn on DLE if the MTU length does not require it.
Then send an HCI_LE_SET_DATA_LENGTH command. A 4.1 device will reject the command as invalid and no response will be received. Sometimes a phone will beat you to it request a DLE data length change before you do. Either way, you will get an HCI_LE_META_EVENT containing a DATA_LENGTH_CHANGE event. The event will contain the new LL packet sizes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.