2020-02-06 10:25 PM
2020-02-09 9:07 PM
Hello,
Are you using the latest SDK on an ST EVAL board ? Kindly specific which board you are using ?
Also, latest Android app is used ?
Kindly check if during the provisioning, the binding to Generic OnOff Model was done or not ?
Hope the "Vendor Model" is not enabled from the menu on the left side of the App. If yes, kindly check to bind the Vendor Model please
Thanks
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.