2020-03-19 5:34 AM
1.Pin21-OE Input terminal of output enable (active low),
Q1-Is this PWM controlled?
Q2-Can use IC without connecting OE pin
2.Pin23-R-EXT Input terminal for an external resistor for constant current programming.
Q1-Can use IC without connecting R-EXT pin.
3.Is this has any over voltage shutdown functionality?
4.Can we connect external over voltage protection circuit ?
We need only SDI,CLK ,LE and over voltage functionality pins to drive LED's
Please let me know if any other IC's can be used for this functionality.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.