2022-10-18 3:32 AM
2022-10-20 7:05 AM
For ST-LINK V2, JTAG cable is used for connection to a standard JTAG 20-pin pitch 2.54 mm connector, and for ST-LINK-V3, Flat cables STDC14 to MIPI10 / STDC14 / MIPI20 (connectors with 1.27 mm pitch)
You can refer to AN4989 for more details
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.