2014-12-18 1:13 AM
We are currently developing a product that uses the SPWF01S module running firmware:
140623-cd34ea1-SPWF01S.Our product relies on the firstset.cgi to connect to a network, the situation is as follows:The problem:
We had this working correctly, but made changes to the code of the microcontroller, that should not affect the described situation, but somehow it does.When using the same webpage, the SPWF01S can no longer connect to WPA2 networks, because is no longer crunches the key:When working correcty:+WIND:28:Station 00:22:43:96:6A:68 Associated
+WIND:29:DHCP reply for 172.31.178.2/00:22:43:96:6A:68
+WIND:29:DHCP reply for 172.31.178.2/00:22:43:96:6A:68
+WIND:57:Received SSID is Network
+WIND:57:Received PWD is Password
+WIND:57:Received Auth mode is 2
+WIND:57:Received Mode is 1
+WIND:2:Reset
+WIND:1:Poweron (140623-cd34ea1-SPWF01S)
+WIND:13:ST SPWF01SA IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.
+WIND:3:Watchdog Running
+WIND:0:Console active
+WIND:46:WPA: Crunching PSK...
+WIND:32:WiFi Hardware Started
+WIND:21:WiFi Scanning
+WIND:35:WiFi Scan Complete (0x0)
+WIND:19:WiFi Join:00:02:6F:AD:AD:18
+WIND:25:WiFi Association with 'Network' successful
+WIND:51:WPA Handshake Complete
+WIND:24:WiFi Up:192.168.10.177
When working incorrectly:+WIND:28:Station 00:22:43:96:6A:68 Associated+WIND:29:DHCP reply for 172.31.178.2/00:22:43:96:6A:68+WIND:29:DHCP reply for 172.31.178.2/00:22:43:96:6A:68+WIND:57:Received SSID is Network+WIND:57:Received PWD is Password+WIND:57:Received Auth mode is 2+WIND:57:Received Mode is 1+WIND:2:Reset+WIND:1:Poweron (140623-cd34ea1-SPWF01S)+WIND:13:ST SPWF01SA IWM: Copyright (c) 2012-2014 STMicroelectronics, Inc. All rights Reserved.+WIND:3:Watchdog Running+WIND:0:Console active+WIND:32:WiFi Hardware Started+WIND:21:WiFi Scanning+WIND:35:WiFi Scan Complete (0x0)+WIND:19:WiFi Join:00:02:6F:AD:AD:18+WIND:25:WiFi Association with 'Network' successful+WIND:40:WiFi DeauthenticationI've checked status and configuration in both cases afterwards and in both causes they seem ok:wifi_mode = 1
wifi_auth_type = 0
wifi_priv_mode = 2wifi_ssid and wifi_wpa_psk_text are correct.The only difference I see is the wifi_wpa_psk_raw being different (due to not being crunched I suspect).What can cause the SPWF01SA to skip this essential step? #spwf01sa-wpa-psk
2014-12-18 4:52 AM
Hi,
you are using a not official FW Release. Where did you get it?I think you are facing an already fixed bug. Please update.Thanksjerry2014-12-18 7:11 AM
Thank you Jerry,
The firmware was suplied to us by silica, who by now have supplied us with a new version: 141106-0950875-SPWF01SCould you tell me if this is the latest/most stable firmware? Because running my current code I already encountered a major bug, the file append command (at+s.fsa=/<filename>,<size>) no longer appends, but overwrites previous data in the file.Again thank you for your time.Jim2014-12-18 7:21 AM
The 141106-0950875-SPWF01S is the latest
official
Release.There is another more recent version, which fix the FSA command issue you found.Please consider this issue as fixed.We'll inform Silica and other distributors when new FW can be delivered.jerry2014-12-19 12:07 AM
Jerry,
Can you give us an estimation on when the new firmware will be available.Considering deadlines we have for this new product, we need to decide to wait for the new firmware, or adept our code to work around the bugs.Thank you,Jim MicolaFrom: gallucci.gerardoPosted: Thursday, December 18, 2014 4:21 PMSubject: firstset.cgi psk not crunchedThe 141106-0950875-SPWF01S is the latest
official
Release.There is another more recent version, which fix the FSA command issue you found.Please consider this issue as fixed.We'll inform Silica and other distributors when new FW can be delivered.jerry2014-12-19 2:33 AM
Hi Jim,
I got your point.A newer version of the FW will be available for customers within Q1 2015.Please consider this issue as already fixed. Could you implement a workaround to avoid the issue? When new FW will be available, this workaround can be removed. Is it ok for you?Thanksj2015-01-05 3:46 AM
We will indeed try to work around it for now.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.