2016-05-02 10:56 AM
With a SPW01SA I'm able to connect to a server using anonymous negotiation, but I often get the following error trying to open a socket before it opens successfully:
ERROR: SSL/TLS Error: Unable to connect (-330)Questions:Exactly what does (-330) indicate?2016-08-26 1:23 AM
Thank you! The first thing that I've noticed is that the CA of the server is changed wrt to the CA you sent to me. You can find it attached or you can control it directly from a web browser.
I have no time today to test it but it seems to be a good candidate for your issue. Let me know! ________________ Attachments : GoDaddyRootCertificateAuthority-G2.pem : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I1RA&d=%2Fa%2F0X0000000bmx%2Fmz.vSlN_f8ZUjd0dvzSEWr7ofdc.UpDd4GkBC2Ee4h8&asPdf=false2016-08-26 10:33 AM
A co-worker mentioned that the certificate we are using is a top-level certificate that completes the certificate chain, whereas the one you attached seems to be second in the chain of certificates. See attached pic.
I found another potential problem. Regarding the TLSDOMAIN command, I found that the domain ''must match the namespecified in the server certificate (Common Name or others). The Common Name in the certificate is applusobd.com, but I was usingwww.
applusobd.com. So now I send: AT+S.TLSDOMAIN=f_domain,applusobd.com<CR> But I still get theVERIFY_SIGN_ERROR. I then loaded the certificate you attached and tried it again. I got the same error. But then I'm guessing that wouldn't work anyway if the server has a different CA certificate. ________________ Attachments : cert_path.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Is&d=%2Fa%2F0X0000000bmz%2FN40.Bfe_6fmXIhI311kJJyKo4o_RdLcJuDlIfPwcZ3g&asPdf=false2016-08-29 12:17 AM
The certificate I've provided to you is a self-signed certificate, so it stays on top of the validation chain. It is possible that the server uses multiple certificate chains.
Try to verify yourself which certificate is used before making a connection with the SPWF01S, for example with a web browser.Regards2016-08-30 3:48 PM
I checked the certificate chain using my browser and found the certificate that you provided (GoDaddyRootCertificateAuthority-G2.pem) was at the top of the validation chain. However, using different computers and even an Android phone, we see different certificates at the top of the chain.
Could you please try to open the socket on your side?
This is what I am sending:AT+S.TLSCERT2=clean,all<CR>AT+S.SETTIME=1472573549<CR>AT+S.TLSCERT=f_ca,1390<CR><GoDaddyRootCertificateAuthority-G2.pem>AT+S.TLSDOMAIN=f_domain,applusobd.com<CR>AT+S.SOCKON=www.applusobd.com,443,s,ind<CR>For me, this leads to the following error:ERROR: SSL/TLS Error: Unable to connect (-188)(-188) ASN_NO_SIGNER_E ASN sig error, no CA signer to verify certificate''This error occurs when using a certificate and the signing CA certificate was not loaded.''We even reinstalled the certificates on the web server and tried opening the socket again. I tried 3 certificates above the server certficate. I am running out of time and my manager insists that you guys should try opening the socket on your end and tell us what is necessary to get it working. I just don't know what to do anymore.2016-09-01 2:22 AM
Hi,
I've checked how the server's certificate is made. Its public key is RSA-4096. As specified in the Application Note AN4683 regarding TLS, the SPWF01 doesn't support these type of certificate (p.11 ''– Public key algorithms: RSA (1024, 2048), ECDSA''). The module wasn't able to establish the connection because the public key was too big.Best Regards2016-09-01 2:32 PM
Thanks so much for the response, and thanks for your patience all this time! We will request new certificates that the module supports.
2017-04-19 10:47 AM
Dear Chris,
About the
'By the way, I'm running into another issue. Sometimes when I send the SETTIME command, the module seems to lock up and then reset. It usually accepts the command when I send it a second time.'
Did you solve it?
Because i am facing the same problem.
The Wifi makes reset sometimes.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.