2023-04-11 4:05 AM
I am looking for a full datasheet for ST microcontroller 324BAAP 269-546 9911L V5 MYS 145. Do you know if I can find anywhere or is any way to ask ST to provide this? Thanks in advance for any help.
Zygi
Solved! Go to Solution.
2023-04-15 3:59 AM
Correct, it is a customised device to which only the respective manufacturer has or had access.
The only chance now would be to contact the respective manufacturer - the success of which is doubtful, however, as it usually involves company secrets.
We are extremely sorry, but in this case we cannot help any further.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards,
/Peter
2023-04-14 12:37 PM
Welcome, @rachas, to the community!
To be able to identify the part, it would be useful to upload a photo here that is as legible as possible.
Regards
/Peter
2023-04-14 1:02 PM - edited 2023-11-20 8:31 AM
Hi Peter, thanks for your reply. Please see attached photo.
2023-04-14 1:50 PM
I suspect it is a custom manufactured part out of the CATANIA M5 fab
Is this in an auto-motive application?
2023-04-14 2:07 PM
Yes, it is an auto-motive application from Bosch part no: 1137328558. It is a radiator fan controller via LIN bus. As far I understand no datasheet is available, isn't it? Do you know another analog for this etc.?
2023-04-15 3:59 AM
Correct, it is a customised device to which only the respective manufacturer has or had access.
The only chance now would be to contact the respective manufacturer - the success of which is doubtful, however, as it usually involves company secrets.
We are extremely sorry, but in this case we cannot help any further.
If the problem is solved, please mark this thread as answered by selecting Select as best, as also explained here. This will help other users find that answer faster.
Regards,
/Peter
2023-04-15 4:03 AM
Thank you ST team for your prompt response.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.