2019-07-30 5:37 PM
2019-07-31 2:01 AM
Hi Ertugrul,
It is possible to create a BLE mesh network with a lot more than 3 nodes.
Good news is you only need 1 element to do that. :)
An element is an addressable entity within a node. Multiple elements are only needed when you physically have more than one entities.
For example, if you design a light fixture with 2 lamps, You may have 2 elements, each implementing an instance of the Light Lightness Server model and an instance of the Generic Power OnOff Server model.
Best Regards,
Winfred
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.