2026-02-06 7:37 PM
I use DTM project,download to my board,but it is not running.I use my project it can running normal.How to solve it ,thanks
2026-03-03 9:09 AM
Hello
Could you elaborate a bit more about setup:
Your own PCB is based on BlueNRG-2 chipset or BlueNRG-M2SP/SA ?
If chipset what is your HW configuration : external 32Khz , RO ? SMPS ?
When flashing DTM you are then willing to connect yo board using BlueNRG GUI over UART ? and connection failed ? If so, the UART mapping on your PCB is same as DTM sample code ?
Thanks
Br
Dominique
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.