2017-02-23 5:35 AM
I have a BlueNRG IDB005V1D board which is connected to its motherboard. I am trying to install firmware onto the STM32L151RBT6 uC on the motherboard but when I am prompted to enter DFU mode there is no LED flashing orange, and and the attempted flash fails.
I tried using the STM32 ST-LINK Utility also to load the DFU_Bootlader.hex but this says that there was no ST-Link device detected. The ST-Link connector that I use does work on another board.
Are there any suggestions as to how I can flash the uC?
Thank you ,
cod
2017-02-27 3:37 AM
I managed to sort this issue using the process detailed in the following link;
http://www.keil.com/support/man/docs/uv4/uv4_fl_hexdownload.htm
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.