2016-03-16 1:38 AM
Hello everyone.
Software: X-CUBE-BLE1 (v. 2.5.2) http://www2.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-ble1.html Example: Sensor Demo Application with DMA and low power mode (Project Name: DMA_LP_SDemo) 1) Equipment: NUCLEO-L053R8 + X-NUCLEO-IDB04A1 - Current consumption in operation mode advertising: about 15 �A - Current consumption in operation mode connections: about 130 �A 2) Equipment: NUCLEO-L053R8 + X-NUCLEO-IDB05A1 - Current consumption in operation mode advertising: about 300 �A !!! - Current consumption in operation mode connections: about 130 �A Power supply voltage 3.3 V. The problem lies in the very high consumption of X-NUCLEO-IDB05A1 mode advertising. Has anyone encountered this problem? #bluenrg-ms-x-nucleo-idb05a12016-03-17 4:40 AM
Dear Customer,
The difference in current consumption observed in Advertising mode is due to different default values for Minimum and Maximum Advertising Intervals used by X-NUCLEO-IDB04A1 and X-NUCLEO-IDB05A1 firmware, respectively. You can tune such values when calling the API: “aci_gap_set_discoverable()�.
Kind regards
AndreaHello everyone.
Software: X-CUBE-BLE1 (v. 2.5.2) http://www2.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-expansion-software/x-cube-ble1.html Example: Sensor Demo Application with DMA and low power mode (Project Name: DMA_LP_SDemo) 1) Equipment: NUCLEO-L053R8 + X-NUCLEO-IDB04A1 - Current consumption in operation mode advertising: about 15 µA - Current consumption in operation mode connections: about 130 µA 2) Equipment: NUCLEO-L053R8 + X-NUCLEO-IDB05A1 - Current consumption in operation mode advertising: about 300 µA !!! - Current consumption in operation mode connections: about 130 µA Power supply voltage 3.3 V. The problem lies in the very high consumption of X-NUCLEO-IDB05A1 mode advertising. Has anyone encountered this problem?2016-03-18 6:09 AM
Thank you for the quick reply.
I set the min and max advertising time. It was just what I needed. Now Current consumption is about 2 µA.
This is the
appropriate value
:)
. I greet and thank youfor your help.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.