cancel
Showing results for 
Search instead for 
Did you mean: 

BlueNRG-2N firmware not working on X-NUCLEO-BNRG2A1

Steven1
Associate II

Hello,

I have the SampleApp running with the BlueNRG-2 firmware on the X-NUCLEO-BNRG2A1. When I reflash the X-NUCLEO-BNRG2A1 with the BlueNRG-2N firmware the SampleApp stops working. It runs again when I switch back to the original firmware.

BlueNRG-2 firmware used:

DTM_SPI.hex

BlueNRG-2N firmware used:

BlueNRG_2N_FW_V3_2_0.bin

Am I missing some configuration steps or something else completely?

Best regards,

Steven

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.