Teseo FL
Good morning,is there a command via I2C bus on TESEO 3FL to activate/deactivate the gpio ANTOFF ?
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Good morning,is there a command via I2C bus on TESEO 3FL to activate/deactivate the gpio ANTOFF ?
HiWe are using part from ST for our Customer product (Lucid Air) - PN: ASM330LHHX But we couldn't find the Top marking standard of part in datasheet. Could you share to me the standard of top marking?
Furthermore, I sent the email requesting activation of the Teseo Suite program but I haven't received the unlock code yet
I want to change the MTU value.As far as I checked through the manual, the mtu value is confirmed through aci_gatt_exchange_config().I want to change the MTU value set at this time.It seems that it can be set when the stack is initialized, but there...
after running the bluetooth low energy expension card, I tried to connect it to the PC to take these parameters through Bluetooth, but the card asks for a code to be able to connect with the PC, does anyone know what the code could be? ,the card is X...
I am trying to program a the BlueNRG1 and i havent been able to find the header files. Is there a link to where I can download those files.
Does STM32 have built-in EtherCAT slave controller?If it is built in, please tell me the model name。 STM32**If it is not built in "What EtherCAT slave controller do you recommend?
Currently I am using ST33HTPH2X32AHE0 for my practice development/testingI was able to read VID_DID, grant access locality, read interface capability I saw it supports 32-byte maximum transfer and burstCount dynamic.In my current setting, because of ...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.