Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X People count

Dear SupporterWe make a design using the "VL53L1X" for people counting applications.To test it, we placed it above the entrance of a room (as in the YouTube link "People Counting Using a Single ST Time-of-Flight Sensor" posted by ST Microelectronics)...

Beacon discovery problem

Hello,I have configured the BLE Beacon V1.0 sensor with the Nano Beacon software, I can detect it with applications like nrf Connect or ST BLE Toolbox. I've programmed a stm32 card as a client, I can detect the devices, but I can't detect the beacon ...

AMACH1_5-1692876253934.jpeg AMACH1_6-1692876261444.jpeg AMACH1_7-1692876501396.png AMACH1_8-1692876580965.png
AMACH.1 by Associate II
  • 882 Views
  • 0 replies
  • 0 kudos

STW81300 PLL Low power at 2.4GHz

Hi all I am using the STW81300 for a project and the Pout level makes sense for 8-16GHz port.  When I set the frequency to 2.4GHz, I am getting only -15dBm or so, while the second and third harmonic of this at 4.8GHz and 7.2GHz are 8dB higher in powe...

mohsenz by Associate
  • 1139 Views
  • 0 replies
  • 0 kudos

S2-LP and LOCKST

Hello,I have an installation where the S2-LP has been blocked in LOCKST(0x14).Which command can remove this ? S2LP_CMD_StrobeReady()?The datasheet doesn't give this information.

Capture d’écran 2023-08-21 164155.png
PCu1 by Senior
  • 1044 Views
  • 0 replies
  • 0 kudos

Resolved! TS555 Reset levels

Hi. From DS of TS555 I'm not clear about RESET acitve low level. In DS VRESET is given 0.4V(min), 1.1V(typ), 1.5V(max) for +25°C and 0.3V...2.0V for whole temp range, see attachementCan someone help to get min/typ/max level for RESET is active and th...

TomLH by Associate
  • 1911 Views
  • 1 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.