Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG-2N bootloader "Get ID" command

Hi,I'm asking the bootloader of an BlueNRG-2N for the "Get ID" command and it responds 0x02 0x01 0x4F.The upper nibble of the last byte ist 4. But 4 is not mentioned in AN4872.4 means ???2 means BlueNRG-20 means BlueNRG-1Any hints?Regards.

H W by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

BlueNRG2 BLE timeout

I am using the BlueNRG2 in an application which is a simple button press to indicate if it is pressed or not. The device needs to connect to Windows 10 and or 11. I am using the SensorDemo project as the base code and made a few changes to just utili...

JWall.1 by Associate II
  • 1940 Views
  • 1 replies
  • 0 kudos

Choosing a Bluetooth Module and Dev Tools

We are looking to add a pre qualified bluetooth module to a consumer product and the device live outdoors and periodically connect to a phone. We have identified the BlueNRG-1 as a candidate but perhaps there is a better choice. How well is the BlueN...

PNada.3 by Associate II
  • 926 Views
  • 0 replies
  • 0 kudos

STUSB1602 firmware problem.

Hello,During testing with the STUSB1602, I encountered strange behavior when using the DRP-mode. Connecting a USB power bank in this mode does not result in a successful connection. Only after pressing the engage-button on a Powerbank, the connection...

Alfredo by Associate II
  • 915 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.