Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ISB027V1 Firmware

Posted on March 15, 2017 at 11:47Hello,I have a problem with the ISB027V1 Eval.Board. I have flashed and erased the Firmware and now I am looking for the File that is mentioned in the user guide WBC_FW_A11 .... but I cannot find it anywhere. Can som...

BlueNRG-MS compatibility with other BLE devices

Posted on March 15, 2017 at 01:59BlueNRG-MS is said to be compliant with Bluetooth standard. However I observed big difference in performance depending on what device connects to BlueNRG-MS. This is how it looks like: iPhone can see the advertising...

grzegorz by Associate III
  • 756 Views
  • 0 replies
  • 0 kudos

STEVAL IDS001V5M and SP1ML868 compatibility

Posted on March 10, 2017 at 16:19Hi,I wanted to try using the sub-GHz radio modules; what i currently have here are 2 evaluation boards:   - A IDS001V5M (SPSGRF-915 module based)   - A SP1ML868 (SP1ML-868 module based)Are they compatible? Can they e...

Spirit1 - SPSGRF-868 high data rate

Posted on February 24, 2017 at 14:27Hi,   I'm working on the module SPSGRF-868 (868Mhz) connected to a PIC24F; the datasheet state that the maximum datarate for FSK is 500Kbps, but after a lot of test I can reach only 100Kbps with frequency dev of 3...

BlueNRG-1 run debug, combine with cc1310

Posted on February 23, 2017 at 13:00Hi ST,I am working with the BlueNRG-1 using STEVAL_IDB and i have few questions please:1- When i program some ST BLE via using Navigatorv2.3.0, the main code not the BLE stack, where it saved? in the main MCU or t...

Nav Dev by Associate II
  • 1539 Views
  • 2 replies
  • 0 kudos

Resolved! BlueNRG-MS device name openly writtable

Posted on May 17, 2016 at 05:24Hi, When the chip is initiated with GAP_INIT, it automatically creates a device name and appearance characteristics. Those are created with write properties, allowing anyone to rewrite the name of the device. I don't f...

hardware by Associate II
  • 2769 Views
  • 6 replies
  • 0 kudos

Mystery chip SP01 P511

Posted on March 03, 2017 at 23:47I have chip on which there's (probably) SP01 P511 (Picture attached). It was manufactured by ST. Probably it's W-MBUS module (or RF in general). I cannot find it anywhere. Do you have datasheet for it?#rf-receiver-tr...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.