Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

USB ESD Protection -> USBLC6-2

Hello,I couldn't find a better category for this.I'm using the USBLC6-2 for USB protection in a product that could potentially have a 20 V USB line (USB-PD). Like this:However, the VDD line would be clamped by this IC, is it acceptable to drop the VD...

0690X000006CBRDQA4.png 0690X000006CBRIQA4.png 0690X000006CBRNQA4.png

Resolved! BlueNRG-1 Wakeup from Sleep

Hi,In my application I put the BlueNRG-1 unit into deepsleep with NO_Timer activated and it can only be awoken by IO12. When the unit is awaken by IO12 I check the wakesource and I confirm it was IO12 that has awaken the chip. Right after this I need...

Multi-connection with Lib BlueNRG-1_2 DK 3.0.0

I try to make multi-connection using BLE lib from BlueNRG-1_2 DK 3.0.0.I cannot connect a second slave device to control after connecting to the first device.The aci_gap_start_general_discovery_proc() failed:0x82Discovery procedure are possible to s...

VKolo by Associate
  • 619 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.