Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Why are all MAC callback functions in I-CUBE-LRWAN moved to lora.c ("inside the stack") and statically defined? (in Stackforce this is not the case)

While working on a standard OTAA Rejoin procedure for our application I've noticed the LoRaMAC callback primitives are all fixed in the LORA_Init() function. When I want to catch the event the MAC layer signals the reception (or not) of a server ACK ...

ingpjb by Associate
  • 710 Views
  • 0 replies
  • 0 kudos

SPIRIT1 CSMA

According to the description of CCA_PERIOD[ ] on page 41 of the ref manual (DocID 022758 Rev 10) , Tcca is the time between two successive CS samplings but the CSMA flow chart on page 40 indicates that CS sampling is done continuously for Tcca durati...

rkris by Associate
  • 1034 Views
  • 1 replies
  • 0 kudos

Converter PLC to CAN Electrical Vehicle

Nowadays I´m working development a converter in PLC (CCS) to CAN (CHAdeMO). But I don´t have sure about the best Evaluation board for this task, because I don´t know frequency in EV and EV supply. I thought EVALKITST8500-1.https://www.st.com/en/eval...

AOliv.13 by Associate
  • 796 Views
  • 0 replies
  • 0 kudos

S2-LPQTR & ISO 18000-6c/EPC Gen2

Just was wondering, would a S2-LPQTR module be able to be used as a transceiver to create a microcontroller based EPC Gen2 RFID (860-960MHz) card?"An Interrogator sends information to one or more Tags by modulating an RF carrier using double-sideband...

admford by Associate
  • 1099 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.