Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STWLC33 - IDE & Advices

Hi,i need to find the right IDE for programming STWLC33 in ISB042V1 Board. Is there any programming advice / code samples in the STM webworld?

roku by Associate II
  • 782 Views
  • 0 replies
  • 0 kudos

I'm starting for a PLC (power line communication ) modem design for transmission over a power line that along his activity can pass from 500 Vac to 24 Vdc or to cold status in a mesh private network .

My question is to verify if the component ST8500 can satisfy what is described previously taking into account that when it has to work with line at 24 Vdc or when in cold status it can't detect any "zero crossing" .Thank you

LPizz.12 by Associate
  • 537 Views
  • 0 replies
  • 0 kudos

Implementing sensor model with bluetooth mesh

I need to implement sensor network with bluetooth mesh having three nodes. Two nodes would be STEVAL-IDB007V1 boards and one of the node would be smartphone which is used to display sensor data from two nodes (STEVAL-IDb007V1) . It is required to col...

MH1 by Associate II
  • 2400 Views
  • 6 replies
  • 0 kudos

List of parts BLUENRG-1 balun

Hello everybody,I designed a board with Bluenrg-1 and discrete balun with the topography draw in the Datasheet.. the problem is that there isn’t a BOM with the value of passives of the balun... where Can I found it? I used the values of the balun of ...

SDK for STream plug.

Hi. I'm trying to design PCB for ST2100, but never worked with this. There is information in quick Start guide about STream plug SDK. Where can i find this?

AZayt.11 by Associate
  • 571 Views
  • 0 replies
  • 0 kudos

GPS chip for embedded application

Hello, could someone suggest me a GPS chip that I can use it with STM32F7 MCU, it should target MCU development not general purpose operation system like Linux or Android and has driver to be implemented inside the MCU firmware.Best regards,Moamen

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.