Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! The Android application crashes, if I compile and run the 1.06 ver, android sample code for BLUENRG-2 SoC in my Android smartphone. What is the solution?

I am using the latest (1.06) android sample code for BLUENRG-2 SoC. After compiling the sample code with MobleLibrary-release.aar library, the apk file is created but when I am running the app in my mobile it crashes. I tried to debug the code and sa...

NKall.7 by Associate II
  • 5151 Views
  • 12 replies
  • 0 kudos

Resolved! Application Freezes when USB is connected

I am using a STM32F746NG which I am attempting to use the STM32_USB_Host_Library. I am able to initialise and start the process fine, but as soon as I connect a USB device to the port the program freezes. I am unsure if the issue is to do with the co...

AfjSpi by Associate II
  • 2672 Views
  • 5 replies
  • 0 kudos

BlueNRG-2 sleep modes questions

Hello, frens!I'm trying to make a BlueNRG-2 application that can send button state just after waking up.I use this code to manage sleep/wake states:if(!APP_FLAG(CONNECTED)) { if(on_sleep_timer == FALSE) { Timer_Restart(&t_sleep); ...

Lenoe by Associate II
  • 1905 Views
  • 2 replies
  • 0 kudos

USB Type-C SPI communication

Hi,I have a control unit that consists of a Cortex M4F, few LEDs, buttons, flash storage and LiPo battery. I also have a PCB with an accelerometer. For now, they are connected with wires and communicating through SPI. When I recharge the device (now ...

unable to wakeup bluenrg by virtual timer

hello,i am using bluenrg 1,and i write code for remote control application.Issues- I called a function to sleep bluenrg1 in main.c , and i used gpio12 and virtual timer to wake-up the device.But device is not wake-up when i put gpio12 at low unless r...

aahme.4 by Associate II
  • 809 Views
  • 0 replies
  • 0 kudos

How i can migrate from F4/L1 to L4?

Hi. I want to connect a STM32L475RG board with an shield,(S2868A1) which comunicated on SPI protocol. More that, i want to connect these 2 components with another Stm32L4 and S2868a1, via S2-LP mode.Can somebody offer me a code or explain how i can m...

cionu by Associate
  • 2215 Views
  • 4 replies
  • 0 kudos

Hello all, I am new user of ST components and am experiencing difficulties to receive MEMS data on SERIAL port of my PC from a the RF 1Ghz module S2868A1. Could you help me understand what is not working properly?

My configuration is the following:Configuration 1 - NUCLEO-F401RE + X-NUCELO-S2868A1 connected on my PC COM3 portConfiguration 2 - NUCLEO-F401RE + X-NUCELO-S2868A1 + X-NUCLEO-IKS01A2 powered by USBI followed the following tutorial:https://www.st.com/...

FJoli by Associate
  • 846 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.