Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG GUI and DK not completely installed

Hi everyone,I tried installing the package "BlueNRG GUI 3.1.0" and I faced certain issues during its installation. First one, there was an issue in driver installation. I am using the STEVAL - IDB008V2 board. But the main issue is with the installati...

0690X000008B9guQAC.png 0690X000008B9hsQAC.png 0690X000008B9jKQAS.png 0690X000008B9jPQAS.png
MagSense by Associate II
  • 3899 Views
  • 9 replies
  • 0 kudos

Appropriate Smartphone for MESH activity

I am trying to select smartphone for MESH activity.Please, tell recomendations for kind of BLE version for smartphone bluetooth adapter.Does either version BLE4.0 is sutable for that, or BLE5.0 and higher is only appropriate?

apronin47 by Associate II
  • 1033 Views
  • 1 replies
  • 0 kudos

Could not initialize BlueNRG-Mesh library! message while trying to do mesh communication using x-cube-blemesh1 package

I am trying to use en.x-cube-blemesh1package with STM32L152RE and X-Nuclueo-IDB05A1 boards. Successfully built the project but while trying to see the data in TeraTerm it is showing Could not initialize BlueNRG-Mesh library!. and also I'm not able to...

Anitha by Associate III
  • 742 Views
  • 1 replies
  • 0 kudos

Having trouble with X-CUBE-SUBG1

Hi, I am using Nucleo-F401RE board, X-NUCLEO-S2868A1 expansion with S2LP and X-CUBE-SUBG1 software. Using code from udp sender and receiver examples, modified to each node be able to send 6LoWPAN message to other node, and answer to message back. Whe...

BlueNRG-1 TEST pin usage

What is the use of TEST pin on BlueNRG-1? STEVAL-IDB007 has a 100K pull-down connected to it, with a jumper that allows a connection to VDD. BlueNRG-MS has it connected directly to GND.Datasheet states that it should be connected to GND, so I expect ...

rastik by Associate III
  • 745 Views
  • 0 replies
  • 0 kudos

C/Q Pin on L6362A

Dear members, reading iO-Link transceiver datasheets like ​for the L6362A i wonder why the Q/C pin and the DI/DO pin are capable of driving loads, i.e. like inductive loads? As far as i understand these pins always are connected to the master, never ...

Two KSZ8851SNL on STM32, working like a hub

I have two KSZ8851SNL connected to an STM32H7 board.In a certain operating mode, I would like to make a 'transparent' connection (on link level) between the two interfaces, so the board with the two interfaces acts like a simple hub.So if I receive a...

Jack3 by Senior III
  • 1186 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.