Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! ST202EB datasheed: table 7 typo?

The ST202EB (ST202EC, ST232EB, ST202EB, ...) RS232 receiver's datasheets shows the following application circuit.Table 7 lists recommended capacitors values for C2-C5 (for the device ST202E is states 0.1 nF, for device ST232 it states 1uF).I think t...

Dan K. by Associate II
  • 1585 Views
  • 2 replies
  • 0 kudos

S2LP trying to implement AUTO-ACK (STack packet)

Hi everyone,(I am using TrueStudio/St-LinkV2)I am using the S2LP on a custom board. Everything worked fine (basic transmission, STack packet) until I wanted to use the auto-acknowledgment feature.Following the procedure (DS, 8.1), I have enabled AUTO...

TClar.8 by Associate II
  • 1073 Views
  • 1 replies
  • 0 kudos

Implementing OTA service for master

We're using two Blue-NRG2 devices and we would like to implement firmware OTA upgrade without using computer. The goal is to read the binary image file through UART by master device, and then send it to slave device via OTA. Upgrading with BlueNRG GU...

Bluenrg Development tools

What software/hardware tools do i need to start developing a custom application on these devices?Can I use the embedded MCU to control a few externals peripheral devices so the bluenrg act as main application processor?

SMakr.15 by Associate II
  • 634 Views
  • 0 replies
  • 0 kudos

BlueNRG V2 and Cube IDE

Hello when i try to import some TrueStudio example from BlueNRG-1_2 DK 3.1.0 into Cube IDE this one ask me to select the correct MCU and the BlueNRG V2 is not proposed ? Any idea ?

FDelp by Associate
  • 749 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.