Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG virtual timer

i checked databook , but couldn't find out the maximum value of HAL_VTimerGetCurrentTime_sysT32();if it's maximum value is max value of uint32_t? (i.e. 4294967295)besides, how to restart the virtual timer?

ann by Associate II
  • 1205 Views
  • 1 replies
  • 0 kudos

X-NUCLEO-S2868A1+long range distance

Hi. i have two STM32F207 with X-NUCLEO-S2868A1.I make working each other with PSP_Demo project. I'd like to check for long distance but i cannot make work.i'm new about sug-ghz, antennas and others.i made it work for about 500 meter in open space wit...

stm32f4 by Associate II
  • 865 Views
  • 0 replies
  • 0 kudos

BlueNRG2 UART TX pullup

Hello,While booting BlueNRG2, I was in need to externally pullup the UART TX output pin for proper operation.The (post) boot initialization examples does not pullup the pin: /* Configure GPIO_Pin_8 and GPIO_Pin_11 as UART_TXD and UART_RXD*/GPIO_InitS...

rnone by Associate II
  • 1666 Views
  • 2 replies
  • 0 kudos

Resolved! Problems to install STSW-BNRGFLASHER on Windows 10

Hi Guys!I'm using windows 7 to programming via SWD the BlueNRG-1.Using this version of windows I don't have any problem. It is my dev PC.But now I need to use on Windows 10 to mass production and change MAC address. The factory only have Windows 10.I...

0690X00000AQPt8QAH.jpg
uilter by Senior
  • 1062 Views
  • 2 replies
  • 0 kudos

Payload format/RawData

Hi,Please find the attached log of BlueNRG - Tile, The out put is taken from a bluetooth router via MQTT.Can you please tell me what is the content of RawData (payload) in the attached file taht is the data indicating which part of output[{"timestamp...

SUT by Associate II
  • 816 Views
  • 0 replies
  • 0 kudos

Saving to NVM on STUSB4500 using STSW-STUSB003

I am porting the STSW-STUSB003 to my STM32 project that uses a different MCU than the NUCLEO-F072RB. Though it wouldn't matter, I need the functionality in our MCU for production, not an external Nucleo dev board.I can make changes in RAM, but cann...

MRex by Associate III
  • 4926 Views
  • 9 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.