Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BlueNRG2 connecting with android app

In one of my project I have to connect my bluenrg2 with custom android app.In order to make this which example code I have to refer?I use BLE-chat example but it couldn't pair from the default bluetooth settings.Then I tried with BLE_SENSOR_DEMO_CEN...

RJOY.1 by Associate III
  • 740 Views
  • 0 replies
  • 0 kudos

BlueNRG-M2 minimum distance to body

Hi everyone,I'm currently using the BlueNRG-M2SP Bluetooth 5.0 module for the design of a body-worn wearable medical device (patch which should be used for up to 7 days). I'd like to know if there's any specification regarding the minimum distance of...

DBer.1 by Associate
  • 530 Views
  • 0 replies
  • 0 kudos

Hi, I designed the PCB where used STUSB4500. I encountered a problem: when I plug USB Type-C connector, USB PD adapter disconnects from my PCB. Could you advise what may reason to disconnect USB PD adapter?

For battery management I using BQ25713Power profiles, which I tried is: 20V 1A (PDO3 default) and 20V 3.25 (also PDO3 manually configured on STUSB4500, this profile appropriate to maximum power of my USB PD adapter 65W 20V 3.25A)This problem exists f...

0693W000003QeLXQA0.jpg
DLyam.1 by Associate
  • 832 Views
  • 0 replies
  • 0 kudos

BLUENRG-M0: number of attributes records

Hello, I'm working with BlueNRG-M0.All is fine when I work with 1 little service. Today I need to implement lot of services and I'm stuck with the error 0x1F from aci_gatt_add_serv() function.My init is this:/*----- CODE -----*/ uint8_t SERVER_BDADDR...

Dams by Associate III
  • 898 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.