Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Can STOTG04ES Exposed pad connected to Ground?

Dear Sir/Madam,I have selected STOTG04ES as replacement for ISP1301BS. Major difference that I could find is the Exposed pad in both ICs. In ISP1301BS should be connected to ground but in STOTG04ES it is NC. Kindly clarify that on connecting to GND ...

B-072Z-LRWAN ACK

Hello,I am using the evaluation board B-072Z-LRWAN with the example code provided by ST (STM32CubeExpansion_LRWAN_V1.3.1), the End Node project. Data is received on my LoRa server, messages are sent as "Unconfirmed". Now, I want to send "Confirmed" m...

0693W000000WVZ6QAO.jpg 0693W000000WVYrQAO.jpg 0693W000000WVYDQA4.jpg
emil28 by Senior
  • 1537 Views
  • 1 replies
  • 1 kudos

St ble NRG2 (BLUENRG-M2SP) : reading the characteristic issue : hi Every one i using BLUENRG-M2SP chip , i using st ble sensor app to communicate the chip , the problem statement , AS below

1. if i read and write  characteristic in the service  its working fine if write one characteristic and read on other characteristic of same service , its not working . after that its not able to reconnect , during this scenario i need to restart ...

mkuma.1 by Associate II
  • 5234 Views
  • 11 replies
  • 0 kudos

Hi, I'm interfacing Nucleo-L476RG with a UART Device. If I power off that devices, my Nucleo code freeze and I need to manually reset it. I need to power-on and to power-off the device and the Nucleo must continue to works.

Nucleo send through UART4 and receive with DMA from devices. Then Nucleo send to PC via USART2 for debugging. In UART4 there is Idle Line detect for receiving unknown length of data.This is my code: MX_GPIO_Init(); MX_DMA_Init(); MX_UART4_In...

FManc.1 by Associate II
  • 856 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.