Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to download STBLESensor Android source code ?

When I try to do then I get fatal error !git clone --recurse-submodules https://github.com/STMicroelectronics/STBlueMS_AndroidCloning into 'STBlueMS_Android'...remote: Enumerating objects: 83, done.remote: Counting objects: 100% (83/83), done.remote:...

LRODR.1 by Associate
  • 899 Views
  • 0 replies
  • 0 kudos

USB OTG FS

We are working on USB OTG FS using stm32H7 customized controller .It is working fine upto 300MHz system clock and unable to create file above 300MHz clock.Is that something I'm missing out in the configuration?

KM L.1 by Associate II
  • 795 Views
  • 0 replies
  • 0 kudos

Where can I get the bin file of WebUSB:CMSIS-DAP?

My PC's OS is Windows 7 64-bit. I had a board IDB011V1. My IDE is IAR 8.40.1. I have installed BlueNRG-LP DK 1.0.0 and BlueNRG-LP Profiles_Lib 1.0.0. Now, I want to build BlueNRG-LP Profiles_Lib 1.0.0 and debug it. But I can not install the driver of...

0693W000007BC9KQAW.png
TWu.6 by Associate II
  • 2143 Views
  • 1 replies
  • 0 kudos

The registers in STuW81300

I have designed a signal source using StuW81300, I want to know when the registers in the chip were set, will the information be lost after power off, and whether it is necessary to reset the register after power on again

JLi.14 by Associate
  • 601 Views
  • 0 replies
  • 0 kudos

BLE card reader with HID sevice

Hi, I use a X-NUCLEO-BNRG2A1 with a NUCLEO-L476RG .My goal is to describe a card reader (USB CCID class) with the HID service. I tested my HID service with the report map of a mouse and it works I can make it move.Now I send the USB descriptors of th...

a28j by Associate II
  • 2005 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.