2018-03-13 1:39 AM
Hello all,
I am facing a problem to update the values when changed. I have an slave bluenrg-1 stand alone which has defined 1 service and 5 characteristics and a master running in coprocessor which has defined 1 service and 5 characteristics.
When declaring service and characteristics everything is fine, I do not get any error.
When I try to update the characteristics from the slave to the master I am using the function aci_gatt_update_char_value() and I received a notification on master but just from one of the characteristics I do not know why I cannot receive the notification from the others characteristics.
Just declaring one of the characteristics, it does not matter which one, I will receive the notification on the master.
2 characteristics have the length of 1 byte, 2 characteristics have the length of 16 bytes and one characteristic the length of 6 bytes.
Anyone has an idea why I am not able to receive all the notifications from the slave?
Thank you
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.