2019-05-30 10:07 AM
Hi all,
there is a way to set a Threshold for VL53L1 and keep the setting even if a power off / power on?
2019-06-03 9:33 AM
There is no user accessible Non-Volatile Memory (NVM) in the VL53L1 sensor. So no, there is no way to keep the threshold if the power is off.
The use case ST envisioned when they invented the sensor is that the sensor would continue to range when the MCU was in low power mode.
The sensor would then interrupt the MCU when the threshold was crossed.
Unfortunately when power is shutdown all the set up information is lost.
But try this...
When you are done ranging, change the Inter-measurement period to a very long time.
The sensor uses only 20 microAmps in the Inter-measurement period.
When you are ready to go again, simply change the Inter-measurement period back to what you had before 'shutting down'.
But if you shut down power completely, you will have to start over completely, and re-initialize the sensor.
2019-06-04 1:06 AM
John, Thank you for your answer.
2019-07-03 4:44 AM
Hello,
Just a little question: what about XSHUTDOWN signal? If we activate it when ranging is required and deactive it when no ranging is required. Is the re-initialization required?
Thanks,
Louis
2019-07-08 10:37 AM
The XSHUTDOWN is almost exactly that - it turns off the chip. And when you turn it back on, you do need to go through the re-initialization step. If you just want to pause a while between ranges, use the Stop and Start commands. Then you will not need to re-initialize.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.