cancel
Showing results for 
Search instead for 
Did you mean: 

Reading distances with VL6180X on the workflow of one shot measurement "Wait for range measurement to complete" SYSTEM__INTERRUPT_CONFIG_GPIO it don't comes set never. what can be the reason?

UDi T.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
John E KVAM
ST Employee

The 6180X is kind of robust but the most common issues are:

  • Poor power.
  • noise on the GPIO0 (Shutdown line) - this puts the sensor into reset and makes mess - a good sized pull-up is recommended.
  • -miss-configured I2C. This is easy to do. Always check the status on all your calls. An i2C failure will show up as a timeout.

But do look at the chip, if it's running you will see the laser - unless you are a bit old. Then use a laptop camera to view the laser.

Good luck,

  • john


If this or any post solves your issue, please mark them as 'Accept as Solution' It really helps. And if you notice anything wrong do not hesitate to 'Report Inappropriate Content'. Someone will review it.
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.