2021-08-02 8:30 AM
If the VDD pin on the left (breakable) part of the breakout board actually is the input voltage, then there is a problem, for the voltage drops and it even causes a brownout.
2021-08-09 4:32 PM
VDD is indeed the input to the sensor - and between 2.8 and 3.3 works. 5V is too high. But if the large chip on the back side of the satellite board is stuffed it's a level shifter and this the satellite board can handle a wide voltage swing.
Enclosed is the schematic for that satellite board.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.