2019-09-05 5:14 AM
I have Nucleo-F446RE and VL53L1x satel. I have connected pins as follow
SCL - D15
SDA-D14
INT-A2
GND-GND
VDD-3v3
When I open GUI software It says Sensor not detected.
2019-09-05 7:24 AM
Unfortunately that is not going to work. The GUI 'talks' to the Nucleo board via the USB serial port interface. We need to load a program onto the Nucleo that converts the serial commands into I2C reads and writes to the sensor. And that program is specific to the Nucleo F401.
One would think you could just buy a Nucleo-F401RE. They are pretty cheap and available. Mouser or Digikey can ship the next day.
But even that is going to be tricky. We put a GPIO expander on the normal expansion board, and so the Nucleo code only works with the expansion board.
So I'm afraid the only real way to run the GUI is with the P-Nucleo-53L1A1 (F401 and VL53L1 expansion board) and it is $56 dollars from Mouser or Digikey (although I've not checked recently).
You could write your own code. The X-cube software from ST will support your configuration. And there are examples in the downloadable API for the VL53L1. But you won't get the fancy graphs.
2019-09-09 7:54 AM
Hi,
You may use the Cube Mx tool to generate a generic code for the F446RE, then copy the existing example code made for F401RE in X-CUBE(X-NUCLEO-53L1A1) from st.com.
thanks,
Julien
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.