2023-03-28 7:24 AM
2023-03-28 7:31 AM
when you range, you can get up to 6000 bytes of information it you want it all. You the the range per zone, the signal strength, a status, some ambient, and you get that for each of up to 4 target per zone.
So at 8x8 x 4 targets all that data adds up.
Look into the platform.h file, there is the number of targets - default to 1. And a host of thing you can disable by uncommenting them.
But you get a lot of data.
Check the number of targets in the zone, then check the status of the target. If you have a target and the status is 5 (6- only occurs on the first range) 9 and sometimes 12 then you know you have something.
BTW, we do the radial to perpenducular conversion for you. When you point the sensor perpendicular to a wall, you will get 64 zones of the same distance. (+/- a few mm)
2023-03-28 7:38 AM
Thank you for your answer! That sounds really interesting. I will look into the platform.h file. Your ToF sensors looks really promising, especially the VL53L8CX!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.