Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

VL53L1X with cover glass needs calibration

HiI am using Vl53L1X to measure dark surface upto 1000 cm far.. I am using a split cover glass(specifications attached). The benefits of using the split cover is that it prevents crosstalk. But even after attaching the cover, the distance measured by...

vl53l1x_cover.jpeg
pthakkar by Associate II
  • 362 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CD due diligence

Hi Community,I’m just finishing off development of a product containing VL53L4CD and need to start to think about approvals etc. ready for product launch. The product as a whole relies on human interaction, so users will be physically close to the pr...

error in vl53l8cx_check_data_ready

 I am currently trying to control a VL53L8CX sensor via SPI communication from the microcontroller mounted on a Crazyflie drone.However, inside vl53l8cx_check_data_ready(), the values in temp_buffer became as follows. Indices [0] to [2] look correct,...

VL6180X API

Hi, I'm supporting a legacy product which uses this older sensor, VL6180X.Where could I find the API source code for download? It seems that all links for "STSW-IMG003", "STSW-IMG011" etc. which are listed in the docs have been erased from the site. ...

pmak by Associate II
  • 341 Views
  • 4 replies
  • 2 kudos

Resolved! Marking on VL53L1X and VL53L1

What is the marking on the bottom side of these sensors i.e. VL53L1X and VL53L1? for eg. on the bottom of VL53L1X it is written VL53LIB...so what is the marking for VL53L sensor. Basically I want to know how can I distuingh between these 2 sensors as...

pthakkar by Associate II
  • 231 Views
  • 1 replies
  • 0 kudos

Resolved! VL53L4CD - readings dependent on target

HiI have been messing around with VL53L4CD for the last few months, and I recently realized that my readings differ significantly, depending on the target color/texture.Here is my setup: The sensor is set on its side, and directly in front of it, at ...

Resolved! VL53L0X offset/xtalk after temperature calibration

Hello, I have a question about the temperature calibration for the VL53L0X Time-of-Flight sensor.The UM2039 manual states the following:> [Temperature calibration] has only to be done before offset and cross-talk calibrations, after Reference SPADs  ...

Resolved! Unstable range results VL53L7CX

This is a continuation from this post, where I erroneously marked the post as solved: https://community.st.com/t5/imaging-sensors/vl53l7cx-distance-data-stratification/td-p/866073Unfortunately I'm still experiencing the issue where range data continu...

jairo1_0-1766853267048.png
jairo1 by Associate II
  • 592 Views
  • 4 replies
  • 0 kudos

Resolved! VL53L4CX multiple objects at longer range?

HeyI've got great success with the VL53L4CX at sorter ranges, but at longer ranges i seem to get two objects. One closeby between 10 and 30mm away, and one at the distance that it should be.I've done calibration and i cant' get this to go away. I'm a...

cyclops by Associate III
  • 297 Views
  • 2 replies
  • 0 kudos

Resolved! Drivers for VD55G0 sensor for STM32N6

Dear all,I'm looking for the driver for the VD55G0 camera sensor compatible with the STM32N657 MCU. According to the camera sensor's driver product page (STSW-IMG505) a driver should be available for the N6 (the N6 is mentioned several times as being...

asdfasdf by Associate III
  • 483 Views
  • 4 replies
  • 0 kudos