Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! VL53L5CX address configuration added to linux driver fork

Hi. I've amended the linux driver for the VL53L5CX with better support for multi-sensor installations, with the I2C address set by the kernel module at initialization, address given by the device tree. ST feel free to add to the official driver, as t...

Poleshift by Associate II
  • 1720 Views
  • 1 replies
  • 0 kudos

Vl53L8CX with STM32WB5mm-DK

I am using Vl53l8cx with stm32wb5mmdk.  I am unable to initialize the sensor via this board. I used  it with a nucleo board and it worked fine, but I need a BLE-based controller to share data. SDA  and SCL are pulled up with 4.7k 3v3 is connected to ...

Rituraj by Senior
  • 1152 Views
  • 1 replies
  • 0 kudos

ToF inaccuracy

Hi,   I was doing a distance test on the VL53L4CX sensor using ESP32 and the ST example codes on Arduino. I'm getting  inconsistent offset errors across the range. The setup is a brine tank with salt inside it. Any ideas on this?   Thank you.

karlacha by Associate II
  • 8403 Views
  • 6 replies
  • 0 kudos

vl53l0x range

hi  I want to use vl53l0/1xv2 as a with rl78 Muc but not getting proper details in data sheet & I am new on STM family so please suggest me the best method for getting high accuracy data

Mak by Associate
  • 7358 Views
  • 2 replies
  • 0 kudos

RingGesture: ToF VL53L5CX for finger and hand gestures

My project makes progress, see here:https://youtu.be/ah19fWodqg8 https://youtu.be/svEeEQ9jmDc My question:When I set LPn low - is just the I2C disabled? Or would also an initiated ranging stop?In order to save power: is there a need to set via I2C th...

tjaekel by Lead
  • 1726 Views
  • 2 replies
  • 0 kudos

VL6180V1

Hi, may I ask you? Is it any difference between STSW-IMG003 (api for VL6180X) and STSW-IMG011 (api for VL6180V1)? Is it working both sensor on same API ? Thank you for replay? Best regards Loring. 

loring by Associate
  • 1496 Views
  • 1 replies
  • 0 kudos