Imaging (sensors)

Discuss applications using ST FlightSense Time-of-Flight sensors, ST BrightSense CMOS image sensors, and ambiant light sensors (ALS) technology. Find answers to your questions on troubleshooting, data accuracy, optimizing communication and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Vl53l1X GPIO1 Interrupt

Hi there,My application is battery operated, so I’m trying to wake up atmega328p from deep sleep from an interrupt though the GPIO pin from the sensor. I'm using Thresholds, "inside window". If any object ditected inside the range, to fire a trigger ...

JPere.3 by Associate II
  • 5336 Views
  • 7 replies
  • 1 kudos

Can multiple VL53L1X be operated in parallel?

Sensors are close to each other (let's say, 30cm). The range is the medium-long one. Their FOV may overlap in production. I'm using ULD. Does this means that I have to VL53L1X_StartRanging and then wait for its result before calling VL53L1X_StartRan...

LDi C.1 by Associate
  • 2321 Views
  • 3 replies
  • 0 kudos

Multiple VL53L1X interrupt mode

For my project, I need to use 2 Vl53L1X on the same I2C bus. The setup is good and i can use them sequentially. But I would like use them in interrupt mode (for have a maximum speed).In short/interrupt mode with one sensor i have 20ms time beetween 2...

Talex.1 by Associate II
  • 3034 Views
  • 5 replies
  • 0 kudos

VL53L1X-SATEL / no blocking function

I connect a vl53l1x-satel to a stm32wb55rg6 with 4 essantial pins (sda, sdl, gnd, vdd). I have a problem to wait for a result. With de function VL53L1_WaitMeasurementDataReady() i haven't problems but for my project I must not use a blocking function...

Talex.1 by Associate II
  • 1212 Views
  • 1 replies
  • 0 kudos

VL6180X range measurement issue

Hello,I have following issue.For distance 0 mm - 60 mm the result of range measurement is always the same (0x20)step by step code:GPIO0 set High.Range measurement start: write 1 to reg 0x0018Wait 100msRead range status: read register 0x004DRead range...

MChla.1 by Associate
  • 1756 Views
  • 2 replies
  • 0 kudos

Resolved! VL53L0X AVDD voltage

Hi everyone,I was wondering if it is possible to supply my VL53L0X with a 3V3 voltage?According to the datasheet, the 3V3 respects the recommanded operating condition.But when I look for example board from ST or other vendors, there is always a conve...

0690X000008iXO0QAM.jpg
Deadror by Associate
  • 4267 Views
  • 4 replies
  • 0 kudos

VL531L1 measurements always FF.

I have rewritten the C app for the VL531 in LAIRD SmartBasic in order to drive the VL531 from a BT module (BL652). I communicate OK with the VL531 over I2C but when I sent the start command (and after I get a Data Ready from register 0x31 as shown be...

TChar.288 by Associate II
  • 2015 Views
  • 2 replies
  • 0 kudos

Resolved! Can we measure the frequency of the beam (VL53L0X) ?

Hello Guys,I hope you all are doing well.I am working on a project that with the VL53L0X ToF Sensor and ESP modules.The sensor works great and i am trying to get deeper into its reads because what i need.I am trying to build a frequency meter using t...

SSilv by Associate
  • 3725 Views
  • 7 replies
  • 0 kudos