cancel
Showing results for 
Search instead for 
Did you mean: 

UM2229 Rev 4 missing details

Xynium
Associate III

HI,

in UM2229 rev4 bottom of page 86/239 it seem value are missing in front of decription "Constellation disabled, Constellation satellites only tracked, Satellites constellation used in position evaluation"

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Francesco Virlinzi
ST Employee

Hi.

You are right, I'l take note to fix it in the next version:

FYI:

0; Constellation disabled;

1: Constellation satellites only tracked;

2: Satellites constellation used in position evaluation

Regards

Francesco

Xynium
Associate III

Ok Tks

 may be an error page 192/239  "Enable/disable the usage of RTC from the GNSS engine. It is recommended to have RTC

usage disabled (Bit12 set to 1) is the RTC crystal is not mounted"

should be (Bit12 set to 0) if disabled or 1 if enabled

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.