2019-12-12 5:52 AM
When boot configuration is set to boot over UART.
How can I use UART0 pins for flashing firmware instead of UART2?
The Xloader 2.2 only recognizes UART2 port for initial firmware flashing.
2019-12-13 1:30 AM
Hi Dror
Booting from UART is running (simultaneously) on all the UARTs.
When the core detects a byte from an UART.... it will go ahead with the whole protocol on the specific UART.
At the end from Host side (or as pins configuration) nothing has to be modified,
Hope this helps
Regards
Francesco
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.