2024-03-16 5:57 AM
Hello!
Can you please help with the differences between Teseo-LIV3FL and Teseo-LIV3F modules, does LIV3FL have all the features of LIV3F plus low power, are there any reasons why to prefer LIV3F over LIV3FL nowadays, or it is recommended to always use LIV3FL instead of LIV3F for new design?
Thanks.
Solved! Go to Solution.
2024-03-18 1:43 AM - edited 2024-03-18 1:44 AM
TESEO-LIV3FL not only has a built-in SMPS and requires less energy than TESEO-LIV3F, but also operates at a lower minimum voltage.
Above all, both are on the 7-year Product Longevity List, but TESEO-LIV3FL will be available for almost 2 years longer:
Hope it answers your question?
Good luck!
/Peter
2024-03-18 1:43 AM - edited 2024-03-18 1:44 AM
TESEO-LIV3FL not only has a built-in SMPS and requires less energy than TESEO-LIV3F, but also operates at a lower minimum voltage.
Above all, both are on the 7-year Product Longevity List, but TESEO-LIV3FL will be available for almost 2 years longer:
Hope it answers your question?
Good luck!
/Peter
2024-04-04 5:24 AM
In addition to the comments above
Teseo LIV3FL has an operating range of 1.8V to 3.3V.
Teseo LIV3FL also supports timing.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.