2025-11-19 8:11 PM
Dear St's engineers,
I am encountering an issue with the GNSS TESEO VIC3DA module regarding the inability to enable the PSTMDRCAL message output. I have tried the command $PSTMSETPAR,1228,0x800000,1*4F (as described in the CDB table 228, which is used to enable three messages: PSTMDRGPS, PSTMDRCAL, PSTMDRSINT), but as a result, only PSTMDRGPS is being output.
2026-02-03 11:36 AM
Hi,
If you are not using wheel tick input or sending speed information over UART, then Teseo VIC3DA is considered in DRUM (Dead Reckoning Unplugged Mode).
The $PSTMDRCAL is only sent when when wheel-tick or speed over UART is present. This is considered DRAW mode. (Dead Reckoning Automotive way)
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.