| Subject | Author | Posted | |
|---|---|---|---|
|
Dear Madam/Sir, We are using powerStep01 and must implement motor "hardstop" purely in hardware (n...
| 2025-02-13 10:25 PM | ||
|
Hi, I’m seeking advice on selecting the appropriate battery monitoring IC for a project involving ...
| 2025-02-09 10:38 PM | ||
|
Hi,
not sure if this is the right section, but:
I have been given an AET-MOT-2DC70S1 motor cont...
| 2025-02-03 7:49 AM | ||
|
Hello, I would like to use the converter SPV1050 in a new product of my company but I have some...
| 2025-01-21 11:10 PM | ||
|
Hello, We are using the STEVAL-L99615C board and encountered an issue while testing the Demo1, Dem...
| 2025-01-20 11:24 PM | ||
|
I am working with the L9961 IC for battery management, and I have a question regarding how the char...
| 2025-01-20 3:57 AM | ||
|
Please confirm, for enable deassertion by long press, PB need to be pressed or both PB and SR needs...
| 2025-01-20 1:09 AM | ||
|
I am planning to use the STM6601 in my design, which involves powering on with a single press and p...
| 2025-01-20 12:57 AM | ||
|
Hi,
Is there driver available for L9966 FlexInput IC ?. Any pointers or code would be helpful...
| 2025-01-16 10:14 AM | ||
|
Hi,
We have ordered the AEK$POW-BMSWTXA Eval board in hopefully testing it with our active batter...
| 2025-01-05 10:21 AM | ||
|
From the datasheet and AN4870, we understand that it is necessary to calculate the battery's intern...
| 2024-12-30 2:30 AM | ||
|
Hi everyone, for this driver I am seeing 700 ns sw deadtime also deadtime: 800. What is difference...
| 2024-12-24 6:03 AM | ||
|
Hi everyone, I’m designing a 3-phase SMPS using the VIPER22A and need some assistance with the tra...
| 2024-12-16 9:59 PM | ||
|
Hi, I am analyzing the different diagnostics capabilities of VNF1048 eFUSE. Could anyone shar...
| 2024-12-09 9:54 PM | ||
|
Hi all, STTH110,the role of the diode in the two-tube forward circuit is the demagnetization of...
| 2024-12-08 4:51 PM | ||
|
Hi all,
I have a problem with the L6924 in the below schematic. After ca. 1 minute of USB pow...
| 2024-12-06 5:52 AM | ||
|
Hi, We are using USBLC6-4SC6 TVS Diode in our design for USB line. The schematic is shown below: ...
| 2024-12-04 4:44 AM | ||
|
Hello, I am currently integrating the STUSB1700 into a custom circuit board design. However, I am ...
| 2024-11-24 4:52 PM | ||
|
Hello, I am working with these two IC's to try and create an SPI programable power distribution ...
| 2024-11-23 12:08 PM | ||
|
Dear Engineer:
Is there an error in the SPI model of SCT1000N170AG_V2?
Why do I have such a sim...
| 2024-11-23 5:01 AM |