| Subject | Author | Posted | |
|---|---|---|---|
|
Which alarm to read if our motor skips steps while moving?
The motor works fine for a period of t...
| 2025-10-06 2:28 AM | ||
|
Hello Team,
We are using VN9E30F High Side Driver, when we try to communicate it through SPI, the...
| 2025-10-05 11:33 PM | ||
|
Hello, I am planning to use the SPV1050 in buck-boost configuration. According to the datasheet, ...
| 2025-10-01 2:21 AM | ||
|
I am debugging a VIPer26-based flyback converter designed, which fails to regulate and is stuck at...
| 2025-09-30 1:28 PM | ||
|
Edited by ST moderator. Please use English language in this community.
HVLED001Aを使用して、150W、AC...
| 2025-09-30 5:06 AM | ||
|
I'm considering developing it with that kit. Can't I download the circuit diagram and firmware f...
| 2025-09-28 7:44 PM | ||
|
Hello I want to control the torque of a PMSM (from a small micro-turbine). I guess that I should u...
| 2025-09-26 6:18 AM | ||
|
Hi Sir, Would it be feasible to achieve an 80A peak current on this board simply by modifying the ...
| 2025-09-23 7:37 PM | ||
|
The SPICE model file for the product SCT040W120G3AG downloaded from the official website is incompl...
| 2025-09-15 8:04 AM | ||
|
Hello experts! my GP is to design an offline DC/DC converter ( LLC ) for cordless home applainc...
| 2025-09-15 7:29 AM | ||
|
Hi,
There is no specific writing description for the cnt bit in the manual.I guess it's the first...
| 2025-09-12 6:28 PM | ||
|
Hello, I have some questions about ISO7637-2 and ISO16750-2 transient pulse simulations using the ...
| 2025-09-11 11:48 PM | ||
|
We’re currently facing an issue with the L4986A PFC controller in one of our designs. The IC is not...
| 2025-09-11 7:34 AM | ||
|
Hello everyone, I would like to use the VND5T016ASP-E high-side driver in my design. For one boar...
| 2025-09-08 11:09 PM | ||
|
IC Part Number _ VNLD5300TR-E
Hi Team, we are using the above IC in our design. If a short c...
| 2025-08-21 1:39 AM | ||
|
Hi, I am using HVLED007 in my 80V, 45W SMPS (Input voltage range 160V-300V). Is it possible for th...
| 2025-08-18 11:18 PM | ||
|
Hi, I was hoping someone may be able to point me in the right direction for two projects I am look...
| 2025-08-16 3:25 PM | ||
|
After visiting the ST website the new GAN 700V Fet's got my attention Part numbers starting with w...
| 2025-08-15 10:34 AM | ||
|
I have been trying to use the EV-VNF1048F with the vnf1048f high side switch on it to act as an SPI...
| 2025-08-13 5:50 AM | ||
|
Hello I am using a STPM801 eval board and will design in the STPM801 on my power management board. ...
| 2025-08-08 8:42 AM |