| Subject | Author | Posted | |
|---|---|---|---|
|
The IO-Link Master (multiport-hub) M12 port on the STEVAL-IDP004V2, has threads on the outside and ...
| 2024-07-29 12:36 PM | ||
|
Hi, I'm beginner in USB-C and USB_PD some things are not clear for me. We developing a device whi...
| 2024-07-24 6:42 AM | ||
|
我尝试使用 STM32L4R9 与 AD7768 通信,使用 8 个通道。我想知道的是:是否可以使用 DCMI 建立 AD7768 与微控制器之间的通信(微控制器支持,但我不确定 AD7768 是否...
| 2024-07-24 1:27 AM | ||
|
Hi,
We try to use STPM34 to measure DC power besides measuring AC power. We had to disable th...
| 2024-07-22 6:10 PM | ||
|
Hi,
We try to use STPM34 to measure DC V and I inputs besides measuring AC. The HPFs of V1,V2...
| 2024-07-21 12:33 PM | ||
|
Hi everyone, I've recently using the BLUENRG-LPS chip for transmitting and receiving data, and I n...
| 2024-07-15 12:15 PM | ||
|
Have a nice day! I use the Bluenrg-2 chip. As the base project, the Power Consumption Test exampl...
| 2024-07-12 8:21 AM | ||
|
I work with a network in which several participants can transmit simultaneously. Each participant c...
| 2024-07-10 8:12 AM | ||
|
Hello; My Name is FATIH I am using Wireless MBUS water meter scanning using S2LP and STM32L073. W...
| 2024-07-09 3:04 AM | ||
|
Hello Everyone, I am using BLUENRG-2 (STEVAL-IDB008V1M) and I have created new 4 custom primary ...
| 2024-07-04 8:59 AM | ||
|
Hi all,
I've just bought a STEVAL-IDB008V2 board, but I don't find any tutorial or ressources lik...
| 2024-07-04 5:25 AM | ||
|
Hi, I am working on the LIS2DU12, but unfortunately it does not yet work as I expected. I do a r...
| 2024-07-03 1:46 AM | ||
|
Hello, this is Lewis I have a question about "STUSB4500 NVM Customer Sector0-4 Write". I would li...
| 2024-07-02 5:30 PM | ||
|
Hi, I'm interested to learn if the BlueNRG-LP chip 355AC can be set in dual mode (which is poss...
| 2024-06-26 12:56 PM | ||
|
Hi all, i have an STEVAL-MKBOXPRO that i want to reprogram. I found STSW-MKBOX-BLEDK here https:/...
| 2024-06-19 1:41 AM | ||
|
Hi I have connected Bluenrg LPS eval board (network coprocessor mode) with STM32L476 Nucleo board...
| 2024-06-17 12:21 PM | ||
|
Hi, during maximum heating tests of our device, we measured a case temperature of +92 °C on the ST...
| 2024-06-13 6:02 AM |