| Subject | Author | Posted | |
|---|---|---|---|
|
Hi We have a custom board using STM32MP257F and would like to program external NIOR flash using...
| 2026-01-05 4:43 AM | ||
|
Hi ST Team, I am working on custom MPU board based on STM32MP257F-EV1 reference design. For our d...
| 2025-12-26 6:27 AM | ||
|
Dear ST Team, We are working on enabling and running the Cortex-M33 core on the STM32MP257F-DK boa...
| 2025-12-15 9:56 PM | ||
|
Hi! I'm going to compile packages to bild a web browser that is optimal for the hardware of MP2. ...
| 2025-12-12 1:26 AM | ||
|
Hi, I'm trying to understand what the viable options are. my goal is to be on more recent versi...
| 2025-12-03 4:18 AM | ||
|
Hello engineers, I'm using the latest version of CubeMX and creating a project with STM32MP135FAFx,...
| 2025-11-20 5:09 PM | ||
|
Hi,
I’m working on a custom board based on the STM32MP157DAC. U-Boot splash is enabled, psplash i...
| 2025-11-12 11:41 PM | ||
|
Cannot boot an m33 TA app from the RFS on a STM32mp257f-DK board running latest OpenSTLinux starter...
| 2025-11-05 5:48 AM | ||
|
Hello, I'm currently testing the security features of OP-TEE and need to use the HUK function of SA...
| 2025-11-05 1:59 AM | ||
|
I'm trying to perform ADC using PA3 (adc1_in15) and PF11(adc1_in2) pins of stm32mp157c-ev1 board bu...
| 2025-10-31 10:45 AM | ||
|
Hello. I am using LVGL to open a USB camera and capture NV12 640*512 video at 30fps. I want to com...
| 2025-10-28 12:08 AM | ||
|
Hi, I’m planning to use OpenSTLinux for an upcoming project and would like to confirm whether it s...
| 2025-10-15 11:59 AM | ||
|
Hello, I am currently using the DDR Utility in STM32CubeProgrammer to tune the DDR4 on my STM32MP2...
| 2025-10-10 5:56 AM | ||
|
Hi I have a board based on a STM32MP135F. I can see that CLK signal of my sdcard (SDMMC1) very ...
| 2025-09-29 9:00 AM | ||
|
Hello everbody! I came across this issue while making a custom Yocto Scarthgap BSP image working w...
| 2025-09-02 2:42 AM | ||
|
Good Evening. I am trying to connect an AI accelerator (ORCA M.2) to STM32MP257F-EV1. I cross compi...
| 2025-08-07 4:00 AM | ||
|
I am currently using a STM32MP157a on an SOC module from aries-embedded and try use the internal AD...
| 2025-08-01 4:12 AM | ||
|
What is FOO driver in https://wiki.st.com/stm32mpu/wiki/Interrupt_overview Interrupts overview shou...
| 2025-07-28 11:50 PM | ||
|
HI With some help from @Gregory PLANCHON and @Olivier GALLIEN I can now boot the processor in M...
| 2025-07-16 9:20 AM | ||
|
As defined in the title, I want to make a clean image for my stm32mp257F-DK without any graphic pac...
| 2025-07-07 8:38 AM |