| Subject | Author | Posted | |
|---|---|---|---|
|
Hello everyone, I am trying to transfer my project generated with motor control workbench from ...
| 2024-09-10 10:17 AM | ||
|
Hello there, I have developed some custom hardware based on the B-G431B-ESC1 and I am looking to c...
| 2024-09-02 6:43 AM | ||
|
Hi,The version of mcsdk I'm using is 6.3.0, I have a problem with my ADC2, enabling one injection c...
| 2024-08-31 3:08 AM | ||
|
Hi, I've been using my custom board with the STM32C011G6 MCU as a control board. By customizing...
| 2024-08-22 9:51 AM | ||
|
Hello everyone I am having a problem when I turn on SPI to display the LED, at the same time I sta...
| 2024-08-16 7:44 PM | ||
|
Dear experts, we like to develop new VFD spindle motor controller, with V/Hz open loop control....
| 2024-08-15 9:55 PM | ||
|
I have made some custom register json file which i want to load in my motor pilot but when i go int...
| 2024-08-15 1:49 PM | ||
|
Hi, I am prototyping a custom PCB with integrated ESC for a BLDC Motor (Datasheet attached). For t...
| 2024-08-09 9:54 PM | ||
|
I just started testing the Motor Control API ,such as the ones below for initializing the motor con...
| 2024-07-31 7:12 AM | ||
|
Hi, has anyone been able to successfully interface the DRV8323HRTAR with an STM32? I have been usin...
| 2024-07-31 5:51 AM | ||
|
Hi, I want to control BLDC motor with X-IHM07M1 motor driver and stm32 nucleo-G071RB microprocesso...
| 2024-07-30 2:08 AM | ||
|
Hey Guys, I am looking to develop a 3 phase motor drive. Any recommendations for an MCU that may c...
| 2024-07-28 9:07 AM | ||
|
Hello everyone, I am generating the observer for an Induction motor with a FOC loop. However, I am...
| 2024-07-26 6:32 AM | ||
|
Hello everyone, I am using the MC SDK AC Induction Motor and I am having some problems with the...
| 2024-07-26 5:40 AM | ||
|
Hi i am New for Arm mbed ,MY project is i want to Control 3 phase induction motor speed using VFD ...
| 2024-07-25 5:12 AM | ||
|
Hello, I'm planning to use 4xSTSPIN32F0 on one PCB and I was planning to use one input supply(3.3...
| 2024-07-25 3:34 AM | ||
|
Good day, my design uses an externally powered STSPIN32G4, so that the CPU can be powered while VM...
| 2024-07-25 12:55 AM | ||
|
Hey everyone, the STM32G4s (including the STSPING4) have the VREFBUF feature, which allows to use ...
| 2024-07-24 1:21 AM | ||
|
Hello, Now I am working on a project for motor control, the MCU is STM32G474VET6, so I started wit...
| 2024-07-23 6:15 PM | ||
|
Hi all, I've been trying to implement a system (due to UL requirement for safety) where I need to...
| 2024-07-22 10:57 PM |