| Subject | Author | Posted | |
|---|---|---|---|
|
I'm trying to read the ID of ST7701SN with STM32F469. The read command was sent correctly by the MC...
| 2025-11-25 7:25 PM | ||
|
Hello everyone, I’m working with the B-L072Z-LRWAN1 Discovery board (STM32L072CZ + Murata CMWX1ZZA...
| 2025-11-12 6:24 AM | ||
|
NUCLEO F411RE, MPU 9250
I'm reading acceleration data via SPI from an MPU 9250 directly to memory...
| 2025-10-10 4:16 AM | ||
|
Hi everyone,
I'm new to the FPV hobby and I've run into a problem that I'm completely stuck on af...
| 2025-10-04 10:12 AM | ||
|
Split from STM32U5G9J DK2 + 4G Module (USB CDC ECM) not detecting USB device - this is a different ...
| 2025-09-26 12:44 AM | ||
|
Hello Community,
I've been trying without success to setup an SPI interface to a LCD panel. It's...
| 2025-09-23 12:51 AM | ||
|
The Raspberry Pi Pico 2W is a dual-core Cortex-M33 processor. It has 16 DMA channels per bus. While...
| 2025-09-22 1:01 AM | ||
|
Hopefully i chose the right thread, right so i have sn stm32h523 chip running a PCISPH fluid simula...
| 2025-08-23 5:05 AM | ||
|
We analyzed the boot and camera initialization time on the STM32N6570-DK using the DCMIPP SnapshotD...
| 2025-08-22 3:34 AM | ||
|
Hello all, I'm currently working on bringing up the CMWX1ZZABZ-078 module from Murata. This module...
| 2025-07-28 11:04 PM | ||
|
Hello, I have a NUCELO_H723ZG and I am trying to set it up to be a master, I am using a MIKROE-3816...
| 2025-07-23 4:11 PM | ||
|
Hello Everybody, I’m developing a Class 0.2 energy metering system for 1-phase, 3-phase (3-wire),...
| 2025-06-28 5:54 PM | ||
|
Hi all, I’d like to share with you a project I recently completed – a digitally-controlled linear ...
| 2025-06-14 10:05 AM | ||
|
I'm working on a DMX communication project using an STM32 microcontroller (e.g., STM32G030K8T6TR). ...
| 2025-05-28 12:47 AM | ||
|
I'm working on a project using STM32U5 and I'm trying to communicate with a TMC2209 stepper driver ...
| 2025-05-23 8:05 AM | ||
|
Hi, I am working on the STM32G431RB and implementing ABI/Z quadrature signal generation. I’m us...
| 2025-05-21 3:41 AM | ||
|
Hi, Printf debugging is a useful tool for software development and it is also a simple way of p...
| 2025-05-15 12:39 AM | ||
|
i want clapping and outside sound provide to the SPH0641LU4H microphone and that is i connected to ...
| 2025-05-09 4:29 AM | ||
|
Hello Guys,
I have a STM32H743IIT6 on a CustomBoard, my Clock is a Quarzoscillator with 25mhz. I ...
| 2025-05-04 3:05 AM | ||
|
I have the NUCLEO STM32F767 developers board and want to use PWM signals from an RC receiver to dri...
| 2025-04-27 8:48 PM |