2025-04-23 4:41 AM
example, viewing the posted message:
But wile editing that message:
But OK again after posting:
2025-04-23 4:46 AM
Oh, it's worse than that!
As you can see, the colon and closing parenthesis are in the wrong order in the posted comment:
So I go to edit it, and put them in the correct order:
But when I post, they get transposed again:
So the forum has converted it to the text form of an emoticon, but then not rendered it as an emoji graphic!
2025-04-23 6:21 AM
Seems to work OK on an initial reply:
https://community.st.com/t5/power-management/stpm01-ic-offset-values-at-zero-voltage/td-p/795844
So just on editing a reply?
2025-04-24 2:21 AM - edited 2025-04-24 4:55 AM
Hi @Andrew Neil ,
Thanks for reporting. I can confirm the behavior during the edit action on my side.
We have a bug registered when emoji interferes with text and code elements which is currently in the fix phase. We are expecting the fix to be done in a couple of weeks.
Once it's completed, we will see if this behavior is fixed too. Will keep you posted on the results.
Apologies for the insolvencies in the meantime.
BR,
Lina
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.