2026-03-27 7:49 AM
144 characters
2026-03-27 7:55 AM
Looks like it should be more like 100 - so that it never has to wrap to a second line in any view.
2026-03-27 8:47 AM
144 is excessive but 100 is good? Eh. We don't need to ride a knife's edge here. 144 is fine.
100 will still wrap if browser is resized, or on phone.
2026-03-27 9:00 AM - edited 2026-03-27 9:23 AM
44% is hardly a "knife-edge" !
Yes, 100 is still "a lot" - could well be shorter.
80 or 72 ... ?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.